Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

The flags have been set in clock synchronous serial I/O mode. ?

Latest Updated:12/05/2008

Question:

The framing error flag, the error sum flag, and other flags are confirmed to have been set in clock synchronous serial I/O mode. Is this correct operation?

Answer:

The only errors that can be detected in clock synchronous serial mode are overrun errors. The framing error and parity error flags are undefined.
Although the framing error or error sum flag may be set, operation will still be correct, because these flags are disabled.
Suitable Products
R8C/1x
R8C/2x
R8C/3x
R8C/Lx
R8C/Mx