Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

TRGIOA output level when count is stopped, timer RG PWM mode

Latest Updated:10/05/2016

Question:

When using timer RG in PWM mode, what is the output level of the TRGIOA pin when the timer count is stopped?

Answer:

If timer count is stopped while using timer RG in PWM mode, the output level of the TRGIOA pin is the initial state (inactive level). The initial state of the TRGIOA pin is determined by the counter clear source.

To change the output level after count is stopped, change the counter clear source using bits CCLR0 to CCLR1 of the TRGCR register. The output level will change at the same time that the counter clear source is changed.

Suitable Products
R8C/36C
R8C/38C
R8C/36M
R8C/38M
R8C/L3AC
R8C/L3AM
  • Was this article helpful?