Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

On the H8S/2345 will /CS0 pin be Low during internal ROM access?

Latest Updated:03/23/2009

Question:

On the H8S/2345 will /CS0 pin be Low during internal ROM access?

Answer:

The /CS0 pin is not LOW during the ROM access. It is Low only when area 0 is accessed as external space.
Suitable Products
H8S/2345
  • Was this article helpful?