Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Is there acceptable level of undershoot for pulse width/power voltage

Latest Updated:04/07/2011

Question:

Is there any acceptable level of overshoot/undershoot (for pulse width and power voltage)?

Answer:

No. There is no acceptable level over or below the specified value. Please use within the range written in the hardware manual (within VIH max and min values).

 

Suitable Products
H8S Family
H8SX Family