Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Is the high level of output ports used in A/D converter VREF or VCC?

Latest Updated:10/10/2008

Question:

(A/D Converter, I/O Port)  When the VCC and VREF values are different, and some of the A/D converter pins are being used as output ports, is the high level of the output VREF or VCC? [2008/10/10]

Answer:

The high level of the output is VCC for these pins. (#107142)
Suitable Products
3803H
3803L
3823
3850A
3858
38D2
38D5
7544
7546
7547