Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Is it possible to debug UART1 using on-chip debugging emulator E8?

Latest Updated:10/10/2006

Question:

When debugging a program using the on-chip debugging emulator E8, is it possible to debug UART1?

Answer:

It is possible to debug pins related to UART1 when using these for some functions (e.g. port etc.) other than UART1.
However, it is not possible to debug the UART1 function. In addition, please do not access UART1 related registers.
Suitable Products
R8C/18
R8C/19
R8C/1A
R8C/1B
R8C/20
R8C/21
R8C/22
R8C/23
R8C/24
R8C/25
R8C/26
R8C/27
R8C/28
R8C/29
R8C/2E
R8C/2F
R8C/2G
R8C/2H
R8C/2J
R8C/2K
R8C/2L