Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Is it possible to change UART1 settings during UART0 operation?

Latest Updated:09/22/2010

Question:

Is it possible to write to the UCON register in order to change the UART1 settings during UART0 operation?

Answer:

It is possible to change the UART1 settings even during UART0 operation. However, you have to over-write the same value to the bits for UART0.
Suitable Products
M16C/62A
M16C/62A(M16C/62T)
M16C/62M
M16C/62N
M16C/62N(M3062GF8NFP, M3062GF8NGP)
M16C/62P
M16C/63
M16C/64A
M16C/65
M16C/6C
M16C/6N4, M16C/6N5
M16C/6NK, M16C/6NL, M16C/6NM, M16C/6NN
M16C/30P
M16C/29
M16C/28
M16C/26A
M16C/1N