Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Is it needed to change program to convert Flash to Mask memory version?

Latest Updated:03/26/2009

Question:

Is it necessary to change a source program when converting Flash memory version to Mask memory version?

Answer:

No, but if you access the register of Flash memory such as writing Flash by user program, please change the program not to access the register of Flash memory at the time of switching to Mask memory version.
Suitable Products
H8/300H Tiny
H8/36109
H8/36087
H8/36064
H8/36049
H8/36037, H8/36057
H8/36014, H8/36024
H8/3694
H8/3687
H8/3672
H8/3664
H8/36912, H8/36902