Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Is it likely to mask software startup interrupt with TRAPA on H8S/2345?

Latest Updated:03/23/2009

Question:

Is it possible to mask a software startup interrupt with TRAPA instruction on the H8S/2345 ?

Answer:

No, it is not possible to do this.
Suitable Products
H8S/2345