Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Is it OK to write A/D conversion related registers during conversion?

Latest Updated:10/06/2010

Question:

Is it all right to write to A/D conversion related registers during A/D conversion (ADST bit = 1)?

Answer:

Please write to A/D conversion related registers while A/D conversion is stopped (ADST bit = 0).

Note that if the ADST bit is set to 0 to forcibly stop conversion, the A/D conversion result is undefined and an interrupt request is not generated. In addition, in the case of the 3x and Lx Series, an Adi register that is not carrying out A/D conversion may also become undefined. So it is recommended that you do not use the values of any of the Adi registers.

[A/D conversion related registers]
3x and Lx Series: ADMOD, ADINSEL, ADCON0 (ADST bit excluded), ADCON1, and OCVREFCR
1x and 2x Series: ADCON0 (ADST bit excluded), ADCON1, and ADCON2

Suitable Products
R8C/1x
R8C/2x
R8C/3x
R8C/38A
R8C/Lx