Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Is a data compared with FlashBlockIVerify function?

Latest Updated:03/20/2017

Question:

Is data compared with the FlashBlockIVerify function?

Answer:

No, it isn't.

<For referencce>
 Flash Memory Self-Programming Library
  V850 Microcontrollers Type 01 [Ver.5.00]
   U18208EJ3V0UM00 (3rd edition)
    2.8 Internal Verification

  V850 Microcontrollers Type 03 [Ver.2.00]
   U18211EJ2V0UM00 (2nd edition)
    2.7 Internal Verification
Suitable Products
V850 Family