Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

In IEBus, can I do the SLVRQ first then the master transmission request?

Latest Updated:12/01/2011

Question:

Regarding IEBus, if a slave reception request (SLVRQ) is received during a master transmission request (such as DR setting, MSTRQ setting), can I first finish the slave reception start processing then resume the master transmission request?

Answer:

Yes, you can.
Issue a master transmission request after performing the slave reception processing.
Note, however, that the MSTRQ setting cannot be performed during a period of 61.7μs (forcible reset period) after defeat in a bus conflict.
(Refer to Caution 1 (p.562) in the manual (6th Edition).)

Suitable Products
V850E2/Sx
V850E/Sx
V850ES/Sx