Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

How to properly write to the flash memory and other relevant documents?

Latest Updated:12/01/2011

Question:

I don't quite understand how to write to the flash memory, even though I have read the User's Manual and other relevant documents.

Answer:

A program cannot be directly rewritten by the user system.
Writing to the internal flash memory is performed using a dedicated programmer and parameter file.
Therefore, you yourself do not need to prepare a writing program.
Writing is performed by connecting to the programmer via the interface circuit described in the device manual.
For the actual writing method, refer to the manual of the programmer (such as PG-FP4).
Suitable Products
V850 Family