Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

How to get the LCD controller to output driver control signals for LCD ?

Latest Updated:03/18/2009

Question:

How do I get the LCD controller to output driver control signals (common or segment) for the LCD ?

Answer:

If you are using the internal LCD driver you must enable the display function activate bit (ACT) turn on the LCD drive power supply (PSW) and connect Vcc to V1 to supply the LCD driver circuit.
Suitable Products
H8/300H Super Low Power
H8/300L Super Low Power
H8/300L
H8 Super Low Power