Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

How is Conter Start Bit STR of TSR on H8/300H is set to 0 in PWM mode of ITU ?

Latest Updated:03/26/2009

Question:

What happens if the Conter Start Bit(STR) of the Timer Start Register on the H8/300H is set to 0 in PWM mode of ITU ?

Answer:

The counter of the corresponding chanel will stop the state of output port and contents of the counter will be retained.
Suitable Products
H8/300H