Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

H8/300H Tiny series: Any products with temperature of -40 to +85 °C

Latest Updated:03/25/2009

Question:

In the H8/300H Tiny series lineup, are there any products with an operating temperature range of -40 to +85 degrees Celsius?

Answer:

Yes, there are products with an operating temperature range of -40 to +85 degrees Celsius in Tiny series. If you want to purchase them, please contact to our local sales or distributors for their availability.
Suitable Products
H8/300H Tiny
H8/36109
H8/36087
H8/36077, H8/36079
H8/36064
H8/36049
H8/36037, H8/36057
H8/36014, H8/36024
H8/3694
H8/3687
H8/3672
H8/3664
H8/36912, H8/36902