Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

External capacitance that can be added to a port

Latest Updated:10/05/2016

Question:

Is there any stipulation about the external capacitance that can be added to a port?

Answer:

Although the value of external capacitance is not stipulated, please take care that the voltage applied to a port from a capacitor does not exceed the absolute maximum rating when the microcontroller power supply is cut off. 
Suitable Products