Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Does timer 1 and timer 2 count starts timing when operation starts?

Latest Updated:01/17/2005

Question:

(Timer)   Timer 1 and timer 2 count start timing and count time when operation starts. [2005/01/17]

Answer:

Count starts from the rising edge (2) after the first falling edge of the count source, after timer 1 and timer 2 operations start (1).
Subject to the operation start timing of the timers and count source, after count starts, the time to the first underflow (3) will be different from the time between subsequent underflows (4). (#105079)

Suitable Products
4286