Does the program fetch to Bank 7 regardless of the bank selection?
Latest Updated:03/08/2012
Question:
The manual describes 4-Mbyte Mode(the memory space expansion mode 2) as "When 4-Mbyte Mode(the memory space expansion mode 2) is selected, the bank selection function allows the user to switch the address space." Does the program fetch go to Bank 7 (program area) regardless of the bank selection?
Answer:
The CPU accesses Bank 7 during the program fetch and there is no bank selection necessary for this access.
Suitable Products
M16C/62N |
M16C/62P |
M16C/63 |
M16C/64A |
M16C/64C |
M16C/65 |
M16C/65C |