Does the product packaged with a write control for a serial programmer?
Latest Updated:03/01/2005
Question:
(Flash Memory) Does the product come packaged with a write control program for a serial programmer? [2005/03/01]
Answer:
Yes. The write control program for a serial programmer is stored in the boot ROM area.
If you plan on using a serial programmer, be careful not to erase the boot area by mistake when reprogramming with a parallel programmer. (#104876)
If you plan on using a serial programmer, be careful not to erase the boot area by mistake when reprogramming with a parallel programmer. (#104876)
Suitable Products
3803H |
3803L |
3850A |
38D2 |
38D5 |