Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Does frequency of oscillation affects the accuracy of A-D conversion?

Latest Updated:07/04/2003

Question:

(A/D Converter)   According to the RC oscillation frequency Ta-f characteristics, the oscillation frequency changes based on temperature. Does this affect the accuracy of A-D conversion?

Answer:

No, oscillation frequency changes will not affect the accuracy of A-D conversion. Please note, however, that A-D conversion time will be affected. (#105011)
Suitable Products
4508
4509