Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Can you name 3 features of H8S that improved power consumption over 300H

Latest Updated:03/23/2009

Question:

Give three hardware features that result in the H8S having improved power consumption over the 300H.

Answer:

"Event driven logic.

Local Clock Pulse Generators at the peripherals so that only one clock phase is distributed around the device. The two phase clock is generated at the peripheral.

Split BUS. For the majority of the time the CPU uses a lowcapacitance bus to access ROM and RAM. When a peripheral needs to be accessed, the higher capacitance peripheral bus is switched in."

Suitable Products
H8S/2668
H8S/2655
H8S/2643
H8S/2633
H8S/2628
H8S/2615
H8S/2612
H8S/2437
H8S/2368
H8S/2398, 2357
H8S/2355
H8S/2350
H8S/2345
H8S/2282, 2280
H8S/2276
H8S/2258, 2239, 2238, 2237, 2227
H8S/2245
H8S/2215
H8S/2214
H8S/2199R
H8S/2194
H8S/2172
H8S/2168
H8S/2158
H8S/2140B
H8S/2114R
H8S/2111B
H8S/2110B