Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Can voltage drop detection circuit be use amid RC oscillation in H form?

Latest Updated:01/16/2006

Question:

(Low Voltage Detection/LVD)   In the H version, can the voltage drop detection circuit be used during RC oscillation? [2006/01/16]

Answer:

Yes. The voltage drop detection circuit is not dependent on the state of oscillation. (#105588)
Suitable Products
4508
4509