Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Can this work area be used as general user's RAM in application system?

Latest Updated:03/26/2009

Question:

Question about work area for flash programming (H'F780 to H'FB7F)
Normally, can this work area be used as a general user's RAM in the application system? (join the work area and user area to be used a 2 byte internal RAM)

Answer:

Yes, you can.
Suitable Products
H8/300H Tiny
H8/36109
H8/36087
H8/36077, H8/36079
H8/36064
H8/36049
H8/36037, H8/36057
H8/36014, H8/36024
H8/3694
H8/3687
H8/3672
H8/3664
H8/36912, H8/36902