Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Can the system be use with some ports open?

Latest Updated:03/25/2009

Question:

When resetting, the ports are initialized for input. When the ports are reset for output after releasing the reset, may I use the system with some ports open?

Answer:

Yes, you can use the system with some ports open, if the ports are reset for output after releasing the reset.
Suitable Products
H8/300H Tiny
H8/36109
H8/36087
H8/36077, H8/36079
H8/36064
H8/36049
H8/36037, H8/36057
H8/36014, H8/36024
H8/3694
H8/3687
H8/3672
H8/3664
H8/36912, H8/36902