Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Can the TxDi pin used as an I/O port?

Latest Updated:03/19/2012

Question:

When only reception is performed using serial interface UARTi, can the
TxDi pin used as an I/O port?

Answer:

By setting the function select register, the TxDi pin can be used as an I/O port.
Suitable Products
M32C/95
M32C/8A
M32C/88
M32C/87
M32C/85
M32C/84
M32C/83
M32C/80