Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Can a program made for use with the 4283 Group be used for the 4286 Group?

Latest Updated:02/05/2009

Question:

(Software, Software Programming)  Can a program made for use with the 4283 Group be used for the 4286 Group? [2009/02/05]

Answer:

Yes, the 4286 Group is software-compatible and pin-compatible with the 4283 Group.
However, some funcations are difference. Please refer to 4283 Group & 4286 Group's datasheets and application notes for the difference. And characteristic values, operating margins, noise tolerance and noise radiation may vary within the range of the electrical characteristics depending on differences in manufacturing process, on-chip ROM, layout pattern, and so on.
When switching and using these products, always evaluate each product system.
Also, consult with the manufacturer of your oscillator to determine the appropriate oscillators and oscillation circuit constants for generating a stable operating clock with your system and conditions. (#107257)
Suitable Products
4286