Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Can Renesas write in or read out code even code protection of QzROM is on?

Latest Updated:01/09/2009

Question:

(QzROM)  When code protection of QzROM is enabled, although I can't write in or read out the code, is it possible for Renesas to write in or read out the code? Also, is there any way to unprotect it? [2009/01/09]

Answer:

When code protection of QzROM is enabled, even Renesas can neither write in/read out nor unprotect the code. (#107245)
Suitable Products
3803H
3823
3850A
3858
38D2
38D5
7544
7545
7546
7547
7548
7549