Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Can PB0/AN0 - PB7‚ /AN7 be set to general input port at the same time?

Latest Updated:03/25/2009

Question:

Can PB0/AN0 - PB7‚ /AN7 pin of H8/3664 be set to the general input port at the same time?

Answer:

No, this setting is impossible. PB0/AN0 pin, as initial value, is set to analog input pin: of eight pins, at least, one should be used as the analog input pin.
Suitable Products
H8/300H Tiny
H8/3664