Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Can I program into parts of the reserved or free areas of the SFR?

Latest Updated:06/06/2007

Question:

(Special Function Register (SFR))  May I program into parts of the reserved or free areas of the SFR? [2007/06/06]

Answer:

Please do not access the reserved or free areas. (Do not change the status after reset) (#106719)
Suitable Products
3803H
3803L
3823
3850A
3858
38D2
38D5
7544
7546
7547
7548
7549