Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Can I check if level is High or Low in Port Register shared w/ TAiout pin

Latest Updated:02/27/2012

Question:

When I select the pulse output function of Timer A in timer mode, can I check if the level is High or Low from the Port Register of the port which is shared with the TAiout pin?

Answer:

Yes, you can check the level of output signals from the Port Register. However, please set the port shared with the TAiout pin as an input port with the Port Direction Register.
Suitable Products
M32C/8A
M32C/88
M32C/87
M32C/85
M32C/84
M32C/83
M32C/80
M16C/62A
M16C/62A(M16C/62T)
M16C/62M
M16C/62N
M16C/62N(M3062GF8NFP, M3062GF8NGP)
M16C/62P
M16C/63
M16C/64A
M16C/64C
M16C/65
M16C/65C
M16C/6C
M16C/6N4, M16C/6N5
M16C/6NK, M16C/6NL, M16C/6NM, M16C/6NN
M16C/5L
M16C/56
M16C/5LD
M16C/56D
M16C/5M
M16C/57
M16C/30P
M16C/29
M16C/28
M16C/26A