Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Are there ready-made standard devices that can transmit in NEC format?

Latest Updated:04/01/2006

Question:

Are they any ready-made, standard devices that can transmit in NEC format?

Answer:

Unfortunately, there are not.
A reference program can be provided. Contact your local NEC Electronics sales representative.
Suitable Products