(R32C/M32C/M16C)What values of external capacitance can be added to the ports?
Latest Updated:06/12/2009
Question:
What values of external capacitance can be added to the ports ?
Answer:
(1) CMOS3 State I/O Ports
When adding external capacitance, select approximately 30 pF (*Note).
*Note:
Value used during measurement of timing characteristics by Renesas.
Please perform evaluations for your system to determine an appropriate capacitance for your system.
(2) Input-only Ports
There are no special restrictions on these ports. Select the capacitance according to the characteristics of the externally connected circuit.
Suitable Products
R8C/1x |
R8C/2x |
R8C/3x |
R8C/Lx |
R8C/Mx |
M16C Family (R32C/M32C/M16C) |