Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

(Pin) What is the initial output level of CNTR0 output? [2007/08/09]

Latest Updated:08/09/2007

Question:

(Pin)  What is the initial output level of CNTR0 output? [2007/08/09]

Answer:

The initial output level of CNTR0 output is high impedance.
When the P12/CNTR0 pin function selection bit (W53) is set to 0, the value of the port P12 output latch is output from the pin.
However, internally, CNTR0 output will be in the initialized high impedance state. (#106689)
Suitable Products
4508
4509