Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

(H8S) Is it possible to set φ output pin as I/O port output pin?

Latest Updated:12/25/2008

Question:

Is it possible to set φ output pin as I/O port output pin?

Answer:

No. φ output pin cannot be set as I/O port output pin. (There is no alternative settings.)
Suitable Products
H8S/2472, 2463, 2462
H8S/2456, 2456R, 2454
H8S/2426, 2426R, 2424
H8S/2378, 2378R
H8S/2368
H8S/2398, 2357
H8S/2355
H8S/2350
H8S/2345
H8S/2339
H8S/2329
H8S/2319