Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

(4559) When leaving unused pins open, how should the output latches be set?

Latest Updated:08/09/2007

Question:

(Pin, I/O Port)  When leaving unused pins open, how should the output latches be set? [2007/08/09]

Answer:

D0-D4: Any value of output format and output latch is acceptable.

D5: Disable INT pin input.
Any value of output format and output latch is acceptable.

P00-P03: Disable key-on wakeup.
Do not set the output latch to 0 when the pull- up transistor is ON.

P10-P13: Disable key-on wakeup.
Do not set the output latch to 0 when the pull- up transistor is ON.

P20-P23: Disable key-on wakeup.
Do not set the output latch to 0 when the pull- up transistor is ON.

P30-P33: Disable key-on wakeup.
Do not set the output latch to 0 when the pull- up transistor is ON.

C: Any value of output latch and CMOS output format is acceptable.
Do not select CNTR input as the timer 1 count source.

(#106686)

Suitable Products
4559