Skip to main content
Renesas Singapore - Knowledgebase

What specific mark should I use for the rubber and the laser marks?

Latest Updated:09/15/2006


[SuperH RISC, H8S, H8/300H, H8/300H Tiny, H8/300L, H8/300, HMCS400] There are two mark specifications (one for rubber stamps and one for laser marks). Which mark specification should I use?


The usable type of mark differs with each MCU used. For information, please contact the nearest Renesas sales office.
Suitable Products
H8/300H Series ROM Ordering
H8/300H Tiny Series ROM Ordering
H8/300L Series ROM Ordering
H8/300 Series ROM Ordering
H8S Family ROM Ordering
SuperH RISC engine Family ROM Ordering
HMCS400 Family ROM Ordering