Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Is the PLP period the same as the product supply period?

Latest Updated:04/01/2015

Question:

Is the PLP period the same as the product supply period?

Answer:

The PLP period is the the duration that "special life cycle management" will be performed. After the PLP period finishes, normal life cycle management will be performed for the product. Under normal life cycle management, the production period is determined based on demand and other factors. If the product is going to enter EOL, Renesas will issue a PDN (Product Discontinuance Notice) in accordance with JEDEC (JESD48B) in advance.
Suitable Products
PLP (Product Longevity Program)