Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Shortage of SCL Clocks to Re-Start Communication After Transmission Interruption

Last Updated:07/04/2018

Question:

After transmission interruption by the simple I2C mode of serial communication interface (SCI) , there is not enough SCL clocks left to re-start communication.
What is wrong?

Answer:

If the stop condition is generated while data still exists in the transmit data register (TDR), the data before the interruption will be outputted when re-starting communication. It is necessary to clear the data in TDR in order to re-start normal communication.

Please reset the setting mode in the following procedure after communication interruption. 
①Prohibit serial transmission/reception(SCR.TE = SCR.RE = 0).
②Clear the bus release and condition request (SIMR3 = F0h).
③If reception data exists in RDR register (SSR.RDRF = 1), read receive data register(RDR).
④Enable serial transmission/reception(SCR.TE = SCR.RE = 1).

Suitable Products
RX Family
  • Was this article helpful?