Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

If Data Inside Internal RAM Is Retained When CPU Is Reset

Last Updated:05/25/2018

Question:

Is the data inside the internal RAM retained when the CPU is reset?

Answer:

We do not guarantee retention of RAM data following a reset during normal operation.

Since a reset occurs asynchronously from normal operation, it could occur while data is being written into the RAM. In such a case, data might not be correctly written into the RAM.

Consequently, if a reset occurs during normal operation, integrity of the data in the RAM cannot be guaranteed.
This is a problem associated with the timing at which a reset occurs. No problem happens if a reset occurs while data is not being written into the RAM. However, if a reset happens to occur while data is being written into the RAM, the amplitude of the write signal might be less than the specified value or the address might fluctuate while the write signal is on. Consequently, data might be written not only into the address that was being written, but also into another address.

Suitable Products
RL78/G10
RL78/G11
RL78/G12
RL78/G13
RL78/G14
RL78/G1A
RL78/G1C
RL78/G1D
RL78/G1E
RL78/G1F
RL78/G1G
RL78/G1H
RL78/I1A
RL78/I1C
RL78/I1D
RL78/I1E
RL78/L12
RL78/L13
RL78/L1A
RL78/L1C
78K Family